Question
I just upgraded from STM32CubeMX V4.24.0 w/CubeH7 V1.2.0 to STM32CubeMX V4.26.1 w/CubeH7 V1.3.0.
When I migrated my project, the Middleware LwIP was grayed out so I could not include LwIP. When I generated code, there were no LwIP files. I looked in the CubeH7 repository and the LwIP files are there. Short of copying LwIP from the repository, how do I enable LwIP in my CubeMX project?