Solved
Is it possible to use only the UART interface of the ST25R3911B-DISCO instead of the USB?
I'm using a ST25R3911B-DISCO for a project and I need to use the UART interface, instead of the USB one and the software provided by ST, to send commands (like INVENTORY, READ BLOCK, WRITE BLOCK) and receive the corresponding information.
Is it possible with this board? And if it is, how can I proceed to implement it?
Thanks in advance,
Eduardo