Skip to main content
joneuhaus
Associate II
March 18, 2008
Question

Count the frequency of 3 external signals

  • March 18, 2008
  • 2 replies
  • 701 views
Posted on March 18, 2008 at 05:58

Count the frequency of 3 external signals

    This topic has been closed for replies.

    2 replies

    joneuhaus
    joneuhausAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hello,

    I would like to measure the frequency of 3 differents signal (max frequency = 100kHz).

    What is the best way to handle this problem?

    > Use the Timers 2,3 and 4 in Input Capture mode and check the value of the counter register each second

    > Use an interruption to detect new pulse

    > Use an external counter and retrieve its value each second (which one?)

    > others ideas?

    Have you some configuration example to use a Timer in Input Capture mode?

    Thank you in advance for your advices.

    joneuhaus
    joneuhausAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    I have used an other way to measure frequency : I use a standard input and retrieve the value each second. Here is the code.

    It works up to 450kHz, on 3 different inputs.

    Here is the main code :

    int main (void)

    {

    /* System Clocks Configuration */

    RCC_Configuration();

    /* NVIC configuration */

    NVIC_Configuration();

    /* Configure the GPIOs */

    GPIO_Configuration();

    /* Configure the USART1 */

    USART_Configuration();

    /* Clear reset flags */

    RCC_ClearFlag();

    /* private variables declaration */

    bool bln_HF1,bln_F1,bln_E1;

    bool bln_HF2,bln_F2,bln_E2;

    bool bln_HF3,bln_F3,bln_E3;

    unsigned int value=0;

    int cpt1=0,cpt2=0;

    /* Infinite loop */

    while (1)

    {

    /* If 1s has passed */

    if(TimeDisplay == 1)

    {

    /* Display counter values */

    printf(''cpt1 : %d / cpt2 : %d/ cpt2 : %d\t'',cpt1,cpt2,cpt3);

    cpt1=0;

    }

    /* Rising edge detection and incrementation of counter 1 (PC1) */

    bln_E1=GPIO_ReadInputDataBit(GPIOC, GPIO_Pin_1);

    bln_F1=~bln_HF1&bln_E1;

    bln_HF1=bln_E1;

    if (bln_F1) cpt1++;

    /* Rising edge detection and incrementation of counter 2 (PB9) */

    bln_E2=GPIO_ReadInputDataBit(GPIOB, GPIO_Pin_9);

    bln_F2=~bln_HF2&bln_E2;

    bln_HF2=bln_E2;

    if (bln_F2) cpt2++;

    /* Rising edge detection and incrementation of counter 2 (PA0) */

    bln_E3=GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_0);

    bln_F3=~bln_HF3&bln_E3;

    bln_HF3=bln_E3;

    if (bln_F3) cpt3++;

    }

    }