Skip to main content
joneuhaus
Associate II
Mar 12, 2008 6:03 AM UTC
Question

Basic conversion function

Posted on March 12, 2008 at 07:03

Basic conversion function

    This topic has been closed for replies.

    2 replies

    joneuhaus
    joneuhausAuthor
    Associate II
    May 17, 2011 10:26 AM UTC
    Posted on May 17, 2011 at 12:26

    Hello,

    I am actually trying to develop a communication between hyperterminal and STM3210 eval board.

    I would like to transmit real/string/integer by an easy way.

    Is there some functions to make this conversions (integer/real >> string)?

    Is there a better way to handle this (something like printf) ?

    Here is my sending routine :

    Code:

    /******************************************************************************* <BR>* Function Name : USART_send <BR>* Description : Send a frame through USART <BR>* Input : const char *s <BR>* Output : None <BR>* Return : None <BR>*******************************************************************************/ <BR>void USART_send(const char *s) <BR>{ <BR> while (*s) <BR> { <BR> USART_SendData(USART2,*s++); <BR> while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); <BR> } <BR>}

    [ This message was edited by: joneuhaus on 12-03-2008 10:13 ]

    joneuhaus
    joneuhausAuthor
    Associate II
    May 17, 2011 10:26 AM UTC
    Posted on May 17, 2011 at 12:26

    I have found a way to do the trick : I use sprintf.

    In the following example, I run an ADC conversion and send the return value through USART.

    int main(void)

    {

    #ifdef DEBUG

    debug();

    #endif

    unsigned int value=0;

    volatile char *b;

    /* Configure the system clocks */

    RCC_Configuration();

    /* NVIC Configuration */

    NVIC_Configuration();

    /* Inputs Configuration */

    GPIO_Configuration();

    /* USART Configuration */

    USART_Configuration();

    /* ADC Configuration */

    ADC_Configuration();

    while (1)

    {

    /* Test if PB.09 level is low (Key push-button on Eval Board pressed) */

    if (GPIO_ReadInputDataBit(GPIOB, GPIO_Pin_9) == 0x00)

    { /* Key is pressed */

    /* Introduction message */

    USART_send(''\r\nHey, you push me!!!\r\n'');

    /* Start ADC conversion */

    ADC_SoftwareStartConvCmd(ADC1,ENABLE);

    /* Wait End of conversion */

    while (!ADC_GetFlagStatus(ADC1,ADC_FLAG_EOC));

    /* Retrieve ADC value */

    value=ADC_GetConversionValue(ADC1);

    /* Convert the ADC value into string */

    sprintf(&b,''valeur = %d'',value); // convert integer >> String for display

    /* Send the previous string through USART */

    USART_send(&b);

    }

    }

    [ This message was edited by: joneuhaus on 12-03-2008 11:34 ]

    [ This message was edited by: joneuhaus on 12-03-2008 11:36 ]