Question
OV7670 and DCMI problem
Posted on July 27, 2014 at 05:18
I have been trying to get the OV7670 cam working with STM32F207zg but seems like something is not clear , first i need to know what is the buffer size to set the DMA to when i want to transfer a snapshot from the cam to External SRAM (since i can not directly send it to the LCD) , say i want 240 * 320 pixels (RGB565) , and the external RAM is 16-bit wide , so what should be the buffer size for the DMA ? ........
also im not sure if the documentation is clear about the VSYNC and HSYNC , the camera module has the VSYNC active high (i,e Data r not sampled when its high) and HSYNC active low , so what should the DCMI settings for VSYNC and HSYNC ? with the following code , i get DMA FIFO ERROR , and I get the frame flag set , but when i display the frame (even if not complete) , the LCD shows noise DMA_InitTypeDef DMA_DCMI; // Configure the DCMI // Enable the Clck of the DCMI module RCC_AHB2PeriphClockCmd (RCC_AHB2Periph_DCMI , ENABLE); // Reset the DCMI Registers RCC_AHB2PeriphResetCmd(RCC_AHB2Periph_DCMI, ENABLE); RCC_AHB2PeriphResetCmd(RCC_AHB2Periph_DCMI, DISABLE); // // Configure the DCMI DCMI_Struct.DCMI_CaptureMode=DCMI_CaptureMode_SnapShot; DCMI_Struct.DCMI_CaptureRate=DCMI_CaptureRate_All_Frame; DCMI_Struct.DCMI_ExtendedDataMode=DCMI_ExtendedDataMode_8b; DCMI_Struct.DCMI_HSPolarity=DCMI_HSPolarity_Low; DCMI_Struct.DCMI_PCKPolarity=DCMI_PCKPolarity_Rising; DCMI_Struct.DCMI_VSPolarity=DCMI_VSPolarity_High; DCMI_Struct.DCMI_SynchroMode=DCMI_SynchroMode_Hardware; DCMI_Init(&DCMI_Struct); // // Enable the NVIC for the DCMI NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_DCMI.NVIC_IRQChannel=DCMI_IRQn; NVIC_DCMI.NVIC_IRQChannelCmd=ENABLE; NVIC_DCMI.NVIC_IRQChannelPreemptionPriority=1; NVIC_DCMI.NVIC_IRQChannelSubPriority=2; NVIC_Init(&NVIC_DCMI); // // NVIC_DCMI.NVIC_IRQChannel=DMA2_Stream1_IRQn; NVIC_DCMI.NVIC_IRQChannelCmd=ENABLE; NVIC_DCMI.NVIC_IRQChannelPreemptionPriority=1; NVIC_DCMI.NVIC_IRQChannelSubPriority=1; NVIC_Init(&NVIC_DCMI); // // Enable the DCMI Interrupts DCMI_ITConfig(DCMI_IT_VSYNC, ENABLE); DCMI_ITConfig(DCMI_IT_LINE, ENABLE); DCMI_ITConfig(DCMI_IT_FRAME, ENABLE); // DCMI_ITConfig(DCMI_IT_ERR, ENABLE); // // // // Enable DMA2 Clock RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); // Configure the DMA DMA_DCMI.DMA_Channel = DMA_Channel_1; DMA_DCMI.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS; DMA_DCMI.DMA_Memory0BaseAddr = 0x64000000; DMA_DCMI.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_DCMI.DMA_BufferSize = 320*240*2; DMA_DCMI.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_DCMI.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_DCMI.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_DCMI.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_DCMI.DMA_Mode = DMA_Mode_Normal; DMA_DCMI.DMA_Priority = DMA_Priority_High; DMA_DCMI.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_DCMI.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_DCMI.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_DCMI.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream1, &DMA_DCMI); DMA_ITConfig(DMA2_Stream1 , DMA_IT_TC , ENABLE); DMA_ITConfig(DMA2_Stream1 , DMA_IT_FE , ENABLE); // Enable the Capture mode DMA_Cmd(DMA2_Stream1, ENABLE); /* Enable DCMI interface */ DCMI_Cmd(ENABLE); /* Start Image capture */ DCMI_CaptureCmd(ENABLE); // // // . . . void DCMI_IRQHandler() { if (DCMI_GetITStatus(DCMI_IT_VSYNC) != RESET) { DCMI_ClearITPendingBit(DCMI_IT_VSYNC); } if (DCMI_GetITStatus(DCMI_IT_LINE) != RESET) { DCMI_ClearITPendingBit(DCMI_IT_LINE); } if (DCMI_GetITStatus(DCMI_IT_FRAME) != RESET) { DCMI_ClearITPendingBit(DCMI_IT_FRAME); for(count=0; count<76800 ; count++) { LCD_REG=0x22; LCD_RAM=BUFF[count]; } } if (DCMI_GetITStatus(DCMI_IT_ERR) != RESET) { DCMI_ClearITPendingBit(DCMI_IT_ERR); } } .. .. Any ideas? ...... Is it cam settings , is it the DCMI ? >>>>>> thx in advance .