Skip to main content
brobinson0000
Associate
May 5, 2013
Question

STM32F105 CAN bus baud rate

  • May 5, 2013
  • 2 replies
  • 834 views
Posted on May 05, 2013 at 10:24

Hi, I am currently working on a project that require to monitor the CAN bus for specific data and once it received the data it will process and store on to flash memory. The data come in high volume bursts.

One of the key requirement is that it has to be low power, I was thinking of throttling the PLL frequency once it finished writing data to flash memory to save some juice, however, this will inadvertently  alter the baud rate of the CAN Bus. Has anyone have experience changing the PLL on fly and still able to receive data from the CAN Bus without missing any data on the network? Any help is much appreciate.

Ben

#stm32f105-can-bus
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 5, 2013
Posted on May 05, 2013 at 13:27

Where is the flash memory, and how is it's write speed materially effected by the CPU speed? Have you benchmarked this?

Changing the clocks on the fly, will likely provide windows of unavailability.

If you can leave the  PLL alone, and change the AHB divisors whilst leaving APB(CAN) alone, or idle with WFI, that might also save some power. Consider also a higher HSE, and not using the PLL.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
brobinson0000
Associate
May 6, 2013
Posted on May 06, 2013 at 11:51

Hi Clive,

The problem lies in the processing of the data, it’s taking a large amount of time and I can’t do post-processing because another node on the network is waiting on the result. But I will take your advice on changing the divisor. Thanks.

Ben