Skip to main content
m__it
Associate III
June 3, 2014
Question

Spi 3 problem STM32F429

  • June 3, 2014
  • 2 replies
  • 734 views
Posted on June 03, 2014 at 11:30

Hello

In our project we need the Spi 3 channel to control an Oled display. The display is connected to pins: D6, B3 and B4 so the Spi 3 pins need to be remapped to those pins.

The remapping is done in the spi3 init function:

void Spi3_Init(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

SPI_InitTypeDef  SPI_InitStructure;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3 , ENABLE);

/////////////

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

GPIO_Init(GPIOB, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_AF_SPI3);

GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_SPI3);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

GPIO_Init(GPIOD, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_SPI3);

///////////////

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 7;

SPI_Init(SPI3, &SPI_InitStructure);

SPI_Cmd(SPI3, ENABLE);           /* Enable the SPI  */

}

After this function is called, we do some basic data sending with this function:

while (1)

{

SPI_I2S_SendData(SPI3, 0x55);

Delay_Ms(10);

}

we did some basic testing with a oscilloscope to check the spi is working but can only see that the clock pin is working. The Mosi pin does nothing. 

If we make a GPIO pin of the Mosi pin we can toggle the pin.

Are there things we have missed? 

My sincerly

    This topic has been closed for replies.

    2 replies

    stm322399
    Senior
    June 3, 2014
    Posted on June 03, 2014 at 11:51

    I know this sounds weird: SPI3 MOSI on PD6 is not an AF_SPI3 (0x06) but 0x05, according the datasheet.

    Change your AF config argument with GPIO_AF_SPI1 (or SPI2, SPI4, SPI5, SPI6)  or simply 0x05.

    m__it
    m__itAuthor
    Associate III
    June 3, 2014
    Posted on June 03, 2014 at 15:25

    That solved the problem! Thank you for the quick response!