Question
L6208 REPLACING GS-D200S
Posted on May 11, 2013 at 21:44
I am working on developing a board to replace the ST GS-D200S with the L6208 for a pre-existing application. I have already designed and manufactured a small amount of boards for this purpose.
I can't seem to get the proper torque out of the motor I am using (datasheet below). The system is running at 2A and 24V. I am not sure of the driving frequency. Also, when the motor is running correctly (although with low torque) it will intermittently seize up and make a grinding noise. I used the suggested component values for the charge pump. My current sense resistors are .3 OHMS/2W. I have a voltage divider of 10k and 1.15k supplying the Vref's which gives a ref voltage of approx. .515. I know this seems like very limited information but if anyone can provide any help I would greatly appreciate it. The specific motor is the HY200 2215 0220 AX04 Motor Datasheet: http://www-app.etsit.upm.es/departamentos/teat/asignaturas/lab-ingel/mpap_hy_lab.pdf #l6208