Skip to main content
stmicro239955_st
Associate II
August 4, 2014
Solved

External RAM SPC564A example project?

  • August 4, 2014
  • 1 reply
  • 826 views
Posted on August 04, 2014 at 17:22

Are there any example projects for the SPC564A on the SPC56xxMB EVAL board that show how to use external RAM?

If not complete projects, any code snippets or even hints or advice?

Thanks

Kevin
    This topic has been closed for replies.
    Best answer by Erwan YVIN
    Posted on August 08, 2014 at 17:13

    Hello Kevin ,

    On the application wizard , there are 5 test applications :

    SPC564Axx OS-Less CAN Test Application

    SPC564Axx OS-Less DSPI Example Application

    SPC564Axx OS-Less eQADC Example Application

    SPC564Axx OS-Less ICU-PWM Test Application

    SPC564Axx OS-Less Test Application

    I am checking with experts about your requests.

    Best regards

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    August 8, 2014
    Posted on August 08, 2014 at 17:13

    Hello Kevin ,

    On the application wizard , there are 5 test applications :

    SPC564Axx OS-Less CAN Test Application

    SPC564Axx OS-Less DSPI Example Application

    SPC564Axx OS-Less eQADC Example Application

    SPC564Axx OS-Less ICU-PWM Test Application

    SPC564Axx OS-Less Test Application

    I am checking with experts about your requests.

    Best regards

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.