Skip to main content
developer2
Senior
August 7, 2013
Question

PWM pausing

  • August 7, 2013
  • 8 replies
  • 1357 views
Posted on August 07, 2013 at 13:52

Hi All,

i'm using on STM32F417 PWM on TIM4 CH2, i have successfully initialized PWM, i have there LED with blinking on 2Hz,

i would like to pause and i would like to return PWM to initial state with configured polarity,

is it possible with one command ?

when i use only TIM_Cmd( TIM4, DISABLE);

the LED stays in the last state, sometimes stays lighting and sometimes stays in off state,

Thank You for all replies,

Kind regards ...

#!telegraphing
    This topic has been closed for replies.

    8 replies

    Tesla DeLorean
    Guru
    August 7, 2013
    Posted on August 07, 2013 at 14:11

    TIM4->CCR2 = 0;  Would be more predictable

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    developer2
    Senior
    August 7, 2013
    Posted on August 07, 2013 at 14:59

    here is my source:

    DEBUG_LED_GREEN1_TIM4CH2(x)

    {

      if(x==0)

      {

       TIM_SetCompare2( TIM4, 0);

       TIM_Cmd( TIM4, DISABLE);

       TIM_CtrlPWMOutputs( TIM4, DISABLE );

      }

      else

      {

       TIM_SetAutoreload( TIM4, x);

       TIM_SetCompare2( TIM4, (x/2==0?1:(x/2)) );

       TIM_Cmd( TIM4, ENABLE);

      }

    }

    still no success :(

    i tried:

       TIM_Cmd( TIM4, DISABLE);

       TIM_SetCompare2( TIM4, 0);

       TIM_CtrlPWMOutputs( TIM4, DISABLE );

    and also:

       TIM_Cmd( TIM4, DISABLE);

       TIM_CtrlPWMOutputs( TIM4, DISABLE );

       TIM_SetCompare2( TIM4, 0);

    :(

    DAS.ANIL KUMAR
    Associate II
    June 20, 2014
    Posted on June 20, 2014 at 09:22

    I have same problem.... i used tim1 ch4 and ch3 i want to start channel3 after 1 us  or delay betwwen ch3 and ch4  of 1 us ....plz help me ..

    thanks

    Tesla DeLorean
    Guru
    June 20, 2014
    Posted on June 20, 2014 at 13:51

    The timers really don't work that way, there is a single counting element and the CCRx are just latches/comparators.

    If you want to impart some phase shift of one channel vs the next, use toggle mode, however this will always give you 50/50 duty unless you actively reprogram the TIMx->CCRx values ahead of the counter.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    DAS.ANIL KUMAR
    Associate II
    June 21, 2014
    Posted on June 21, 2014 at 08:14

    thank u for reply .............. how can i shift the phase  for 1 us delay.between these channel signal . which register value used for phase shift  ..i am using stvd and stm8s103.......thanks .

    Tesla DeLorean
    Guru
    June 21, 2014
    Posted on June 21, 2014 at 14:28

    What's with the periods?

    This is an STM32 forum, if you have an STM8 question post it to that forum.

    If I had a 72 MHz system clock, with no prescaler 1us would be 72 ticks, and to get a phase shift in toggle mode you'd advance one CCRx by 72 with respect to the other.

    TIM1->CCR1 = N;

    TIM2->CCR2 = N + 72; // modulo period as required

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    DAS.ANIL KUMAR
    Associate II
    June 23, 2014
    Posted on June 23, 2014 at 07:19

    thank u sir,   i didnot find phase shift in stm8 foroum thats why i am here.........i am using 16 Mhz internal freq.  i am generating  both signal with 10us for on and 8 us for off and continue and i want to 1 us second delay between these signal  or 2nd sinal start after 1us and continue.

    plz help me   thanks

    Tesla DeLorean
    Guru
    June 23, 2014
    Posted on June 23, 2014 at 14:47

    thank u sir,   i didnot find phase shift in stm8 foroum thats why i am here.........i am using 16 Mhz internal freq.  i am generating  both signal with 10us for on and 8 us for off and continue and i want to 1 us second delay between these signal  or 2nd sinal start after 1us and continue.

     

    plz help me   thanks

    Then open a new question in the STM8 forum, the two platforms are not compatible.

    Failing that you'll have 2 rtfm.....

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..