Skip to main content
stm32
Visitor II
May 26, 2013
Question

adding USB interface descriptor

  • May 26, 2013
  • 1 reply
  • 666 views
Posted on May 26, 2013 at 19:53

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    1 reply

    tsuneo
    Associate II
    May 28, 2013
    Posted on May 28, 2013 at 02:13

    IAD (Interface Association Descriptor) should be applied to bind the interfaces on the original class, when it comes up in a composite device together with another interface(s).

    By the USB spec, Audio may bind with other interfaces without IAD. But without IAD, Windows seem to allow limited classes of additional interfaces, such as HID.

    Tsuneo