Skip to main content
m2399
Associate
June 1, 2013
Question

problem with jtag tck pin

  • June 1, 2013
  • 2 replies
  • 687 views
Posted on June 01, 2013 at 08:55

hi

I have a problem

with jtag tck pin on my board.

When

I touch

it with

my

finger

  the st-link

Works properly

& connect to stm32f417 but if  i remove my finger from this pin the st-link not connect to my mcu.i pull-down tck pin with 10k to gnd.

Also, when

i connect my board's gnd to pc case

this

problem

can be

solved

.

What is

the problem?why tck pin is sensitive to the touch of my finger

???
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    June 1, 2013
    Posted on June 01, 2013 at 13:39

    Sounds like some supply connectivity issues, perhaps a schematic and diagram of the connections made would be illustrative.

    How is the board powered? How are grounds on the ST-Link connected to your board.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    m2399
    m2399Author
    Associate
    June 2, 2013
    Posted on June 02, 2013 at 06:45

    i convert (2*10 )jtag connector to  header (1*7)  & only use

    NRST

    TDI

    TDO

    TCK

    TMS

    GND

    VDD

    on my board.also don't use JTAG TRST & pull-up it on my board