Question
CubeMX tool generates dubious declaration for periph init.
Posted on September 27, 2015 at 16:07
Hi,
when I generate code for the STM32L0 in CubeMX, my compiler discovers the following problem:~/projecten/SunnaBat/software/Controller/toepassing/cube/SunnaBat/Src/adc.c:149:47: error: declaration of 'hadc' shadows a global declaration [-Werror=shadow]void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc)
^
~/projecten/SunnaBat/software/Controller/toepassing/cube/SunnaBat/Src/adc.c:45:19: note: shadowed declaration is here
ADC_HandleTypeDef hadc; Same deal with other peripherals like IDWG or I2C. The generated software has a local variable named exactly the same as a global variable! This is a recipe for confusion or worse. My compiler is arm-none-eabi-g++ (I won't use gcc, since most of my code is c++) Has anybody found a way to make the tool generate proper function variable names? I can change them by hand but every time I re-generate from the tool I lose my changes and I need to do it all again. Perhaps ST could test the code with a c++ compiler, they are much more strict on typechecking and names than a c compiler. Thanks, Ewout Boks