Skip to main content
rothkalman
Associate
September 4, 2014
Question

STM32f302RCT6 Y revision package marking problem

  • September 4, 2014
  • 2 replies
  • 814 views
Posted on September 04, 2014 at 14:44

Dear Forumers!

I've just started to solder in the pcb components into my pcb. I have a MCU as in the title mentioned, and I've faced a problem about the chip placement. In the official drawing the package only contains one marking circle, but in the reality the plastic chip package has two orientation marks:

A smaller and deeper left from the ST logo and a bigger and less deeper one above the ST logo.

First I've assumed that the first marking marks the no. 1 pin, but after soldering it and applying the voltage on it, the chip started to eject smoke and now acts as a short cut on the pcb. I have a remnant chip remained and I'd like to know which marks signes the first pin of the controller?

I have no battery option so Vbat is floating, and VDDA comes the same time as the VDD. I think this cannot cause this fatal error.

Any idea?

Thanks in advance!
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    September 4, 2014
    Posted on September 04, 2014 at 15:47

    I've used this thread to show various packages and where the designator is. 

    https://community.st.com/0D50X00009Xka68SAB

     

    Edit: Fixed DEAD LINK, original post from 4-Sep-2014

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    rothkalman
    Associate
    September 4, 2014
    Posted on September 04, 2014 at 20:03

    Thank you, that helped me a lot!