Skip to main content
pestov
Associate III
January 11, 2014
Question

st-link/v2 + OS X (10.9.1)

  • January 11, 2014
  • 6 replies
  • 2192 views
Posted on January 11, 2014 at 12:01

How can I debug stm32 apps by st-link/v2 on Macintosh?

Where are drivers of st-link/v2 for OS X Mavericks?

#stlink-macintosh-st-link/v2-ma
This topic has been closed for replies.

6 replies

chen
Associate II
January 13, 2014
Posted on January 13, 2014 at 11:52

Hi

''How can I debug stm32 apps by st-link/v2 on Macintosh?''

You need a toolchain for Machinosh! As far as I am aware - there are not any.

You could try one of the virtualisations (eg VMWare) to run a PC emulation on the mac.

pestov
pestovAuthor
Associate III
January 14, 2014
Posted on January 14, 2014 at 03:43

hi!

I build/compile project in eclipse + GNU ARM Plugin + GNU Toolchain for ARM

I'm looking for OpenOCD binaries for Mac OS X

chen
Associate II
January 14, 2014
Posted on January 14, 2014 at 11:54

Hi

''I'm looking for OpenOCD binaries for Mac OS X''

I am not sure you understand what OpenOCD is.

OpenOCD is a 'debugger' - it is a 'dongle' that interprets debug commands and communicates with a target processor.

A OpenOCD binary will be targeted to an implementation (hardware)

http://www.amontec.com/openocd.shtml

Or you build your own, that is the point of open hardware.

This connects to the ARM processor so you can debug on it.

On top of that, you need an application that will talk to the OpenOCD so that you can debug. The application will :

download the binary into the ARM

Interpret you source code with the assembler at the current program count.

Set, clear breakpoints.

Allow you to control execution flow (run, step, step into, step over etc)

''I build/compile project in eclipse + GNU ARM Plugin + GNU Toolchain for ARM''

This is only the tool chain that builds the binary.

pestov
pestovAuthor
Associate III
January 14, 2014
Posted on January 14, 2014 at 15:51

Hello!

I build/compile my C projects for stm32 in Eclipse by arm-none-eabi

In MS windows I debug this projects in Eclipse + OpenOCD. I've downloaded OpenOCD binaries for Windows from http://www.freddiechopin.info/en/download/category/4-openocd

Now I want do it in Mac OS X, but can't find OpenOCD binaries for OS X.

Where can i find it?

chen
Associate II
January 14, 2014
Posted on January 14, 2014 at 16:07

Hi

Do not know.

Did you search the internet?

I found this page if info :

http://www.rau-deaver.org/MacOPENOCD.html

pestov
pestovAuthor
Associate III
January 14, 2014
Posted on January 14, 2014 at 19:21

I have done it on Mac!

Open On-Chip Debugger 0.7.0 (2014-01-15-00:11)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.sourceforge.net/doc/doxygen/bugs.html

shutdown command invoked

Info : This adapter doesn't support configurable speed

Info : STLINK v2 JTAG v17 API v2 SWIM v0 VID 0x0483 PID 0x3748

Info : Target voltage: 2.901239

Info : stm32f4x.cpu: hardware has 6 breakpoints, 4 watchpoints

How?

brew install openocd