Skip to main content
dibs
Associate III
August 3, 2014
Question

False Framing Errors?

  • August 3, 2014
  • 5 replies
  • 1033 views
Posted on August 03, 2014 at 23:35

I am using an STM32F407 to receive data via UART and seem to be getting false FE interrupts. There are two reasons why I believe that they are false:

  1. I have looked at the timing on an oscilloscope and it appears to be fine.
  2. If I disable the interrupt, I can receive the data intact with a passing CRC.
Specs:

USART6

1.8432MBaud (I have also tried 115.2kBaud)

8E2

    USART_InitStructure->USART_BaudRate              = BAUDRATE;

    USART_InitStructure->USART_WordLength          = USART_WordLength_8b;

    USART_InitStructure->USART_StopBits                 = USART_StopBits_2;

    USART_InitStructure->USART_Parity                     = USART_Parity_Even;

    USART_InitStructure->USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStructure->USART_Mode                = USART_Mode_Rx | USART_Mode_Tx;

InitUSART(&USART_InitStructure);

USART_ITConfig(USARTx,USART_IT_ERR,ENABLE); 

Any ideas what conditions could be causing this?

#framing-error #stm32f4 #usart
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
August 3, 2014
Posted on August 04, 2014 at 01:13

Well you'd probably do better using a logic analyzer, and toggling a GPIO bit when you see the error, and then try to correlate the two.

Do you need 2 stop bits? Is the next start bit falling within the stop zone? Is it recognizing a glitch as a start bit, and then rejecting it?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
dibs
dibsAuthor
Associate III
August 12, 2014
Posted on August 12, 2014 at 14:23

After some looking, I have solved my problem. ST UARTS include the parity bit as the MSb in the data bits. So 8E2 needs to be set up with a 9 bit word, not an 8 bit word.

I am getting this information from RM0090 Rev6: CR1->PCE bit explanation

Am I correct in this assessment?

I did not expect this to be the case; I expected that the parity bit would be found after the MSb of what we call the data byte, not to be the MSb of the data byte. Is there a standard implementation for this?

Tesla DeLorean
Guru
August 12, 2014
Posted on August 12, 2014 at 17:05

Yes, 8-bit + parity is configured as 9-bit in STM32 implementation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
dibs
dibsAuthor
Associate III
August 13, 2014
Posted on August 13, 2014 at 20:03

Do you know if this is a normal way of doing it or something strange the ST does?

Tesla DeLorean
Guru
August 13, 2014
Posted on August 13, 2014 at 21:01

I think it simplifies the silicon implementation. Others might mask it by having multiple bits documented to support 7N1, 7O1, 7E1, 8N1, 8O1, 8E1, etc or hidden it in the API.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..