Question
Bugreport Cube32MX 4.0 & HAL_UART_TxHalfCpltCallback
Posted on August 02, 2014 at 08:21
Hi,
In the HAL documentation, stm32fxx_hal_uart.c & .h, I can read that in interrupt mode, the HAL_UART_TxHalfCpltCallback is called after half of tx is transfered but this is wrong.The HAL_UART_TxHalfCpltCallback is only called if I use DMA transfers. Either is the documentation wrong or the function is not implemented to end.