Question
Stm32f4cube 1.11.0 have a bug
Posted on February 11, 2016 at 07:05
when I enable USB host and FatFs , Init function in Main created . But it dose not work
int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_ADC1_Init(); MX_ADC2_Init(); MX_CRC_Init(); MX_FSMC_Init(); MX_IWDG_Init(); MX_SDIO_SD_Init(); MX_SPI1_Init(); MX_SPI2_Init(); MX_SPI3_Init(); MX_TIM1_Init(); MX_UART4_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); MX_USART6_UART_Init(); MX_FATFS_Init(); // <<<<<<< MX_USB_HOST_Init(); // <<<<<<<this 2 function must be in a task.