Question
OV2640 camera CIF mode ??
Posted on October 09, 2015 at 22:56
Hullo guys,
Im using the OV2640 sensor to stream video and everything worked fine when it is in the default UXGA mode. My images are 320*240 pixels, so I wanted to move to the CIF mode for faster frame rate . The problem is that the datasheet is a real mess and I'm not sure what I might be messing . I have the following registers with the corresponding values : {0x12, 0x10} // CIF mode {0x18, 0x43}{0x19, 0x00}{0x32, 0x09}{0x03, 0x06}{0xc0, 0x32}{0xc1, 0x2A}{0x50, 0x00}{0x51, 0x64}{0x52, 0x54}{0x53, 0x00}{0x54, 0x00}{0x57, 0x00}{0x5a, 0x50}{0x5b,0x3c} {0x5c, 0x00}//// Those are the values that I changed from the previous working UXGA mode . Any ideas?