Question
DMA SDIO TX underrun error
Posted on March 08, 2014 at 14:46
I got the DMA working fine with SDIO , i can read multiple blocks ok , but when i try write multiple blocks , i get TX underrun error in the SDIO , and i can also see that there is a FIFO error in the DMA , which i do not see when reading from the card ......... any suggestions ?
#lmgtfy:-firmware-library