Question
STemwin GUI_Init Hard Fault
Posted on December 18, 2014 at 11:43
Hullo guys , This is my first time to use STemwin GUI library , everything compiled fine , and the code is simple enough just to test it
int main (){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE); GUI_Init(); GUI_SetColor(GUI_RED); while(1) { }}but the GUI_Init always is giving me hard fault , but tracking the Assembly I found that the reason is the Branch statement to memory address out of scope .I increased the Stack size to 16 KB and it's still not working . GUI_Init calls GUI_X_Config and GUI_X_Init and I can get into these function while debugging , so the error occurs after the execution of these two functions . Any Suggestion ?