Question
STM32F4 USB HID Change PID (Product ID) during runtime
Posted on September 15, 2014 at 15:18
Hi,
Im using the STM32F4 with the STM USB Stack and the demo VB project from
. Communication is working fine.Now I want to change the PID on the STM during runtime. Calling the HidD_GetHidGuid() from the PC,
still shows the old device path name, unless if I detach and attach the USB connector physically.Is there any possibility:
- to force the PC to reimport the HID Device Descriptor?
- generate 'something' in the STM32F4 USB Stack to force the PC to reconnect the USB device?Optionally I could disconnect from the VBUS, changing the special function of the PortA9 to input
pin and reassign it to VBUS, but I'm concerned that this could have a side effect, if the time betweendisconnect and connect is too short, or either too long.I would appreciate a software based solution, without modifying the I/O of the MCU.
cheers
#stm32f4-usb-hid-pid