Skip to main content
ramon13666
Associate II
January 9, 2017
Question

TIM1 registers read errata

  • January 9, 2017
  • 5 replies
  • 1856 views
Posted on January 09, 2017 at 10:00

0690X00000605XvQAI.png

So, info in reference manual is irrelevant? The read should be always done as:

; Read Seq_1
ld A, TIM1_REGH;
ld XL, TIM1_REGL;�?�?�?

?

Will the following sequences lead to incorrect results?

; Read Seq_2
ldw X, #TIM1_REGH; Store in X address of TIM1_REGH
ld A,(X); Read TIM1_REGH
push A;
incw X; Set pointer to TIM1_REGL
ld A,(X); Read TIM1_REGH�?�?�?�?�?�?
; Read Seq_3
ldw X, #TIM1_REGH; Store in X address of TIM1_REGH
ld A,(X); Read TIM1_REGH
push A;
ldw X, #TIM1_REGL; Store in X address of TIM1_REGL
ld A,(X); Read TIM1_REGL�?�?�?�?�?�?�?�?
�?

#stm8-timer
    This topic has been closed for replies.

    5 replies

    Max
    ST Employee
    January 19, 2017
    Posted on January 19, 2017 at 10:42

    Hello,

    In the three code snippets you are referring too, the only multiple cycle instruction is the INCW X you have in the Read seq_2

    As a consequence Read seq_1 and Read seq_3 are OK, but you should not use Read seq_2 for 16-bit TIMer access.

    This also means that the recommendation in the RM is correct.

    If you want to check if an instruction execute in multiple cycles, please refer to

    http://www.st.com/content/ccc/resource/technical/document/programming_manual/43/24/13/9a/89/df/45/ed/CD00161709.pdf/files/CD00161709.pdf/jcr:content/translations/en.CD00161709.pdf

    .

    The Table 42 page 64 to 74 has a column showing the number of cycles.

    Let me know if this is still not clear

    ramon13666
    Associate II
    January 19, 2017
    Posted on January 19, 2017 at 11:24

    This is from doc linked by you:0690X000006065QQAQ.png0690X00000605yfQAA.png

    1 cycle or 2? Where the truth?

    And for Seq_3: ldw is 2 cycle instruction. It's used to load TIM1->CNTRL to index register.0690X000006065RQAQ.png0690X000006065VQAQ.png

    in Seq_1 I've made mistake. LD could not load from memory to XL.

    So, none of this three reads will assemble or return correct result.

    Currently I'm using ''mov _store_mem, _read_mem

    mov _cnt_hi, TIM1_CNTRH
    mov _cc_hi, TIM2_CCR1H
    mov _cnt_low, TIM1_CNTRL
    mov _cc_low, TIM2_CCR1L�?�?�?�?

    Does it get the job? Because I don't know how peripheral feature could be impacted by instruction size or exec time. And what if I have 5-10-20 single cycle instructions between reading High and Low registers?

    Arlet Ottens
    Associate II
    March 19, 2017
    Posted on March 19, 2017 at 13:19

    I tried it out on a STM8S103F3P6 rev Y, and no matter what I do, I cannot get the timer read to return the wrong answer, as long as I read TIM1_CNTRH before TIM1_CNTRL. I even tried reading CNTRH, calling a function to write that value to the UART, reading CNTRL, and it was still correct. 

    My test procedure: stop counter, write 0xffxx to CNTR, start counter, handful of NOPs, and then read CNTRH/CNTRL in various ways. Repeat with incrementing start value. At some point, you'll see the timer roll over.