Skip to main content
abbas
Associate III
March 15, 2018
Question

STM32F103C8t - CAN problem

Posted on March 15, 2018 at 22:24

Hello guys!

I am new in using CAN interface, and for the first time, I started to use it in my project. I used STM32F103C8t. When I wanted to use CAN interface, there only happens time-out exception in run-time and I figured it out both in run-mode and then in debug mode. I wrote a very small project to work on it and I got the same problem. I doubted if the mcu is not working well, I changed it and still not change, I even changed the mcu with stm32f103cBt one and no change either.

I give you the simple code I created using HAL library and STM32Cube here and I hope you can help me

this is the code:

In this code if CAN works, the relay must toggle almost in 10HZ frequency, and if time-out happens the relay must toggle in 1Hz frequency. In practice, the relay toggles in 1Hz!!!

CAN_HandleTypeDef hcan;

CanTxMsgTypeDef    can_tx_msg;

CanRxMsgTypeDef    can_rx_msg;

uint8_t can_tx_buff[8];

int main(void)

{

  /* USER CODE BEGIN 1 */

    char *msg = 'salam';

  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */

  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_CAN_Init();

  /* USER CODE BEGIN 2 */

    hcan.pTxMsg = &can_tx_msg;

    hcan.pRxMsg = &can_rx_msg;

  /* USER CODE END 2 */

  /* Infinite loop */

  /* USER CODE BEGIN WHILE */

  while (1)

  {

        sprintf( (char *) hcan.pTxMsg->Data, '%s', msg );

        hcan.pTxMsg->DLC = strlen(msg);

        HAL_CAN_Transmit(&hcan,1000);    

        HAL_Delay(100);

        HAL_GPIO_TogglePin( relay_test_GPIO_Port, relay_test_Pin );

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

  }

  /* USER CODE END 3 */

}

/**

  * @brief System Clock Configuration

  * @retval None

  */

void SystemClock_Config(void)

{

  RCC_OscInitTypeDef RCC_OscInitStruct;

  RCC_ClkInitTypeDef RCC_ClkInitStruct;

    /**Initializes the CPU, AHB and APB busses clocks

    */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = 16;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;

  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL16;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

    /**Initializes the CPU, AHB and APB busses clocks

    */

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

    /**Configure the Systick interrupt time

    */

  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

    /**Configure the Systick

    */

  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

  /* SysTick_IRQn interrupt configuration */

  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}

/* CAN init function */

static void MX_CAN_Init(void)

{

  hcan.Instance = CAN1;

  hcan.Init.Prescaler = 16;

  hcan.Init.Mode = CAN_MODE_NORMAL;

  hcan.Init.SJW = CAN_SJW_1TQ;

  hcan.Init.BS1 = CAN_BS1_1TQ;

  hcan.Init.BS2 = CAN_BS2_1TQ;

  hcan.Init.TTCM = DISABLE;

  hcan.Init.ABOM = DISABLE;

  hcan.Init.AWUM = DISABLE;

  hcan.Init.NART = DISABLE;

  hcan.Init.RFLM = DISABLE;

  hcan.Init.TXFP = DISABLE;

  if (HAL_CAN_Init(&hcan) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  }

}

/** Configure pins as

        * Analog

        * Input

        * Output

        * EVENT_OUT

        * EXTI

*/

static void MX_GPIO_Init(void)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  /* GPIO Ports Clock Enable */

  __HAL_RCC_GPIOA_CLK_ENABLE();

  /*Configure GPIO pin Output Level */

  HAL_GPIO_WritePin(relay_test_GPIO_Port, relay_test_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin : relay_test_Pin */

  GPIO_InitStruct.Pin = relay_test_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

  HAL_GPIO_Init(relay_test_GPIO_Port, &GPIO_InitStruct);

}

#stm32f103c8t #can-interface
This topic has been closed for replies.

5 replies

T J
Senior III
March 15, 2018
Posted on March 15, 2018 at 23:31

If you don't have a transceiver chip, then you must pull up the CanRx pin, or the processor will hang at startup.

if you can single step, can you see the chip working upto a point ?

abbas
abbasAuthor
Associate III
March 16, 2018
Posted on March 16, 2018 at 10:37

I forgot to say that, I used MCP2551 as CAN transceiver and I mounted this IC on the board like this(forget 100nF in RX, I hadn't assign true value for it at that time):0690X0000060A92QAE.png

and besides, I tested my code at loop-back mode in which, apparently, there is no need for external electrical connections, but I didn't get any result

About your question, I changed the code to this

  while (1)  {

        sprintf( (char *) hcan.pTxMsg->Data, ''%s'', msg );

        hcan.pTxMsg->DLC = strlen(msg);

        HAL_CAN_Transmit(&hcan,10);    

}

and I didn't see any activity at mcu CAN output. After it, I unmounted the MCP2551 chip and put a 10K pull-up resistor and I checked it again and still no output!

T J
Senior III
March 16, 2018
Posted on March 16, 2018 at 13:39

I started with a third party transceiver, the CanDo unit.

I made it transmit every second, until I had the receiver working.

Then I worked on the transmitter code.

________________

Attachments :

image001.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxt5&d=%2Fa%2F0X0000000b1r%2FSHSsvxUyauWbgi3owlYmHWp.mub.JuUc5a9SY6Mijmo&asPdf=false

image002.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxt0&d=%2Fa%2F0X0000000b1s%2FM.yXvzpko9QTcjtIcIJczaZhx5KLtuuPCHF9MMF2X.E&asPdf=false
Tesla DeLorean
Guru
March 15, 2018
Posted on March 15, 2018 at 23:33

Have transceivers and something at the end of the cable to talk too, and respond/acknowledge reception.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
abbas
abbasAuthor
Associate III
March 16, 2018
Posted on March 16, 2018 at 10:40

No clive, but as I responded to T.J., I even tested the CAN in loop-back mode and I didn't get any result