Skip to main content
abbas
Associate III
October 23, 2016
Question

STM32Cube FATFS Problem in STM32F103

  • October 23, 2016
  • 1 reply
  • 919 views
Posted on October 23, 2016 at 21:38

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    1 reply

    abbas
    abbasAuthor
    Associate III
    October 24, 2016
    Posted on October 24, 2016 at 07:18

    Solved,

    The problem was in SDIO Clock Division

    its default value is 0 and it is usually too fast for SDCard to work with. I tested with 6 instead of 0 and it worked.

    The size of stack memory also should be higher than its default value(0x200)... I tested with 0x800 and it worked