Solved
M24LR-DISCOVERY SW documentation
Posted on October 10, 2016 at 12:42
Hello,
I am trying to create an application SW using M24LR-DISCOVERY using RF transceiver board to read devices containing M24LR dual eeprom, but I am struggling to get the documentation to implement functions like the M24LR-DISCOVERY SW has like auto-detect, read memory from - to.... etc. The only documentation I've found are AN3375 Application note and AN3163 Application note. Is there any docs explaining which function and which parameters I need to use to get any result. example: detect and read from EEPROM address 0x15 - CR95HFDLL_USBconnect() - CR95HFDll_SELECT() - CR95HFDll_SendRec() Thanks, Sasa