Question
sdcc 3.5.0 rc1
Posted on June 11, 2015 at 18:18
sdcc 3.5.0 is to be released soon. There already is release candidate 1.
You can download the release candidate and have a look at it. The more eyes on it, the less likely are hidden bugs. The main changes from previous sdcc 3.4.0 are: * Many fixes and improvements in the stm8 port * --disable-non-free configure option * z80 port fixes * long long fixes * Changed default language dialect from --std-sdcc89 to --std-sdcc99 * Reorganized and updated manual * Reduced memory consumption (most noticeable for high --max-allocs-per-node) * Faster compilation for stm8 (most noticeable for high --max-allocs-per-node) * atoll() function for conversion of strings to long long * __z88dk_fastcall and __z88dk_callee calling conventions for more efficient function calls and better compability with z88dk * --lospre-unsafe-read renamed to --allow-unsafe-read Due to the substantial improvements, in particular in the stm8 port, I think all STM8 programmers will want to change from 3.4.0 to 3.5.0. Philipp