Skip to main content
lorenzo
Associate II
February 11, 2009
Question

STM32 and system bus

  • February 11, 2009
  • 3 replies
  • 931 views
Posted on February 11, 2009 at 05:16

STM32 and system bus

    This topic has been closed for replies.

    3 replies

    christophe239955_st
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:02

    If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :o

    lorenzo
    lorenzoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:02

    Hello all,

    I need to interface a CS8900 to STM32, so i need to use the system bus. Can I use the system bus unused pins as GPIOs?

    Thanks,

    Lorenzo

    lorenzo
    lorenzoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:02

    Quote:

    On 11-02-2009 at 00:07, Anonymous wrote:

    If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :o

    Thank you!

    L