Question
Winding noise during hold
Posted on October 25, 2013 at 00:06
Hello,
With L6472 I hear audible (high pitch) noise from motor when holding. volume of noise increase with increase hold current. It does not matter if the motor is loaded or not.
When I look at winding with scope one pair is the typical pwm signal locked and duty cycle appropriate for the hold setpoint
The other pair of windings appear ‘unlocked’ and much higher in frequency than the other winding.
EVAL Bd hardware
24v supply, current set point .35ampNema17, 18mh / 8.9ohms, 0.9degree step angle
Is there a setting I am overlooking
This does not occur with L6470.
thanks for your support !