Skip to main content
February 7, 2016
Question

stm32F746-disco USB HS chip very hot

  • February 7, 2016
  • 0 replies
  • 445 views
Posted on February 07, 2016 at 16:43

Hi All!

We know, what stm32f746 use ULPI whith

USB3320C-EZK to realise USB HS.

I could not run the Demonstration project and any other projects, relating to the USB HS.

And I am surprised that USB3320C chip really hot, very straight.

I want to ask: it must be heated or I did something with meals and it burned down.?

I can add: if power the board from USB st-link, the feeling is that the board does not have enough voltage: this I see on the screen flicker, and if the processor is loaded, the screen may not light at all.

Now I feed giving 5V power supply separately..

It seems to me that I had somehow what is burned chip.

Thanks!

#stm32f746discovery
This topic has been closed for replies.