Skip to main content
a239955
Associate
October 8, 2013
Question

L6470, move and speed change

  • October 8, 2013
  • 1 reply
  • 691 views
Posted on October 08, 2013 at 11:09

Hi.

Using L6470 I need to move to absolute position with the possibility to change speed during motion. I need the Soft Stop (or something similar) when reaching the target.

Speed change during motion is possible using Run command but not using Move command (Move has the deceleration I need when reaching the target).

I already tried 2 solutions but I don't like them both:

1) Using Run and checking continuously if the motor is approaching the target position to issue a Soft Stop at the appropriate time. This is tricky because speed changes often and the ''stop time'' varies accordingly.

2) Using Run + Hard Stop when reaching target pos: this is a mechanical stress to avoid.

Is there any another possibility I'm missing?

Thank you in advance

Alessandro

#absolute-position #speed #l6470
This topic has been closed for replies.

1 reply

Enrico Poli
ST Employee
October 14, 2013
Posted on October 14, 2013 at 15:24

Dear Alessandro,

The solution 1) is the only one fitting your requirements (speed changes often).

In this case the MCU must continuosly evaluate the number of steps reqired to stop according to the deceleration and the motor speed.

Regards

Enrico