STM32f103 timer parallel synchronisation
Hey Everyone
Using ahttp://www.mikrocontroller.net/part/STM32F103
RB I want to use Tim2 and Tim3 for generating a PWM, and want to start them both together such that they run prefectly in sync. Unfortunately, this canonic case I didn't found described in the ref manual or timer AN, so I did some code myself which however doesn't work exactlyas wished. In addition to the timers I use I2C, which I implemented with the CPAL_V1.2.0 library, which hangs up when I use ''my'' sync method. Error/problem description: (1) When I use only I2C then I2C works perfectly. (2) When I use I2C and Tim2 and Tim3 WITHOUT my timer-synch-routine, i.e. when both timers are each started with TIM_Cmd(TIMx, ENABLE), then I2C works perfectly. (3) When I use I2C and Tim2 and Tim3 WITH my synch-routine, then everything works fine as long as I do NOT switch on the timer outputs by writing to TIM2->CCER und TIM3->CCER. (4) As soon as I write to the CCER registers, then the I2C hangs up sooner or later (within few couple seconds). (the timer do work as they should) I'm on this issue since quite some time now without success. In a hope that someone has an answer, Olli Appendix: code fragments/*this is the routine which starts the troubles and eventually makes
the I2C to hang up*/void
motors_onoff_update() { uint16_t tim2_ccer, tim3_ccer; tim2_ccer |= (uint16_t)(1
<<4
) | (uint16_t)(1
<<8
) | (uint16_t)(1
<<12
); tim3_ccer |= (uint16_t)(1
<<0
) | (uint16_t)(1
<<4
) | (uint16_t)(1
<<8
); TIM2->CCER = tim2_ccer; TIM3->CCER = tim3_ccer; }void
timer_init(void
) { GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBase_InitStructure; TIM_OCInitTypeDef TIM_OC_InitStructure;//Initialize clocks for TIM2, TIM3
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE);//Initialize clocks for GPIOA, GPIOB, AFIO
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);//Configure pin TIM2 CH2-CH4 = PA1,PA2,PA3, TIM3 CH1-CH3 = PA6,PA7,PB0 as alternative function push-pull
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure);//Configure TIM2, TIM3 time base
TIM_TimeBase_InitStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBase_InitStructure.TIM_CounterMode = TIM_CounterMode_CenterAligned1; TIM_TimeBase_InitStructure.TIM_Period =1024
-1
;//11kHz with F100RB, 35kHz with F103RB
TIM_TimeBase_InitStructure.TIM_Prescaler =0
; TIM_TimeBaseInit(TIM2, &TIM_TimeBase_InitStructure); TIM_TimeBaseInit(TIM3, &TIM_TimeBase_InitStructure);//Configure TIM2, TIM3 waveform
TIM_OC_InitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OC_InitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset; TIM_OC_InitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset; TIM_OC_InitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC_InitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High; TIM_OC_InitStructure.TIM_OutputState = TIM_OutputState_Disable; TIM_OC_InitStructure.TIM_OutputNState = TIM_OutputNState_Disable; TIM_OC_InitStructure.TIM_Pulse =512
; TIM_OC2Init(TIM2, &TIM_OC_InitStructure); TIM_OC3Init(TIM2, &TIM_OC_InitStructure); TIM_OC4Init(TIM2, &TIM_OC_InitStructure); TIM_OC1Init(TIM3, &TIM_OC_InitStructure); TIM_OC2Init(TIM3, &TIM_OC_InitStructure); TIM_OC3Init(TIM3, &TIM_OC_InitStructure);/*using the following to sync the timers makes the I2C to eventually hang up, see above*/
//Set Master/Slave such to synchronize both timers at enable
TIM_SelectOutputTrigger(TIM2, TIM_TRGOSource_Enable); TIM_SelectMasterSlaveMode(TIM2, TIM_MasterSlaveMode_Enable); TIM_SelectInputTrigger(TIM3, TIM_TS_ITR1); TIM_SelectSlaveMode(TIM3, TIM_SlaveMode_Trigger); TIM_Cmd(TIM2, ENABLE);// TIM_Cmd(TIM3, ENABLE); //is enabled by TIM2
/*if one would NOT use the 4 commands to sync the timers, but would enable Tim3
using TIM_Cmd(TIM3, ENABLE) then everything works perfectly*/ }