Skip to main content
bobdeschambault9
Associate III
March 10, 2015
Question

How to detect MCU at run time?

  • March 10, 2015
  • 8 replies
  • 2200 views
Posted on March 10, 2015 at 14:57

Hi,

Is there a way to determine which MCU is being used on a board?  We are developing software for an STM32F4 and some of our tools are using the 407 and others are using a 429.  I would like to know when our code is running on a given MCU.

Thanks,

Bob
    This topic has been closed for replies.

    8 replies

    Tesla DeLorean
    Guru
    March 10, 2015
    Posted on March 10, 2015 at 15:39

    There's DBGMCU_IDCODE and you can read the flash size from it's location in the System ROM

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bobdeschambault9
    Associate III
    March 10, 2015
    Posted on March 10, 2015 at 18:25

    I notice that the values are the same in the header for both chips.  Is this like some sort of address that contains the chip part number if I read it correctly?

    Tesla DeLorean
    Guru
    March 10, 2015
    Posted on March 10, 2015 at 19:15

    printf(''IDCODE:%08X FLASH:%04X\n'', *((uint32_t *)0xE0042000), *((uint16_t *)0x1FFF7A22));

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jpeacock
    Associate
    March 10, 2015
    Posted on March 10, 2015 at 21:08

    Two places for CPU info.  Look at the SCB->CPUID register for general Cortex processor info.  This will tell you if it's an M0, M3 or M4 (and presumably M7).

    ST has two library routines: DBGMCU_getDevID() and DBGMCU_GetRevID() for ST specific models.  Those help with errata that are rev specific.

      Jack Peacock
    bobdeschambault9
    Associate III
    March 10, 2015
    Posted on March 10, 2015 at 21:39

    Thanks for the information.  I am using ST Cube v1.4 and I looked up the call, it now called ''HAL_GetDEVID()'' and returns a 32 bit unsigned integer.  There is also ''HAL_GetREVID()'' call as well.  The functions are found in stm32f4xx_hal.c.

    waclawek.jan
    Super User
    March 10, 2015
    Posted on March 10, 2015 at 23:56

    > I notice that the values are the same in the header for both chips. 

    What header?

    What values?

    JW

    bobdeschambault9
    Associate III
    March 11, 2015
    Posted on March 11, 2015 at 03:31

    The header files:

    stm32f407xx.h

    stm32f429xx.h

    The values:

    #define  DBGMCU_IDCODE_DEV_ID                ((uint32_t)0x00000FFF)

    #define  DBGMCU_IDCODE_REV_ID                ((uint32_t)0xFFFF0000)

    waclawek.jan
    Super User
    March 11, 2015
    Posted on March 11, 2015 at 09:17

    The values:

    #define  DBGMCU_IDCODE_DEV_ID                ((uint32_t)0x00000FFF)

    #define  DBGMCU_IDCODE_REV_ID                ((uint32_t)0xFFFF0000)

    Ah, I see. These are only masks, indicating the dev ID and rev ID fields in the 32-bit

    DBGMCU_IDCODE

    register.

    Have you already read the content of DBGMCU_IDCODE? Does it match the values from RM0090?

    JW