Skip to main content
sukrubahadirarslan
Associate II
October 7, 2013
Question

stm3210C-Eval Debug-HSEStatus

  • October 7, 2013
  • 3 replies
  • 616 views
Posted on October 07, 2013 at 08:59

hello forum. I am new at arm so first I want to use the GPIO. I use stm3210c-eval. and this development board use stm32f107VC. I write code like this.

#include ''stm32f10x.h''

#include ''stm32_eval.h''

#include <stdio.h>

GPIO_InitTypeDef GPIO_initstructure;

void delay(void)

{

uint8_t i,j;

for(j=0;j<250;j++)

{

for(i=0;i<250;i++);

}

i=0;

j=0;

}

/**

  * @brief  Main program.

  * @param  None

  * @retval None

  */

int main(void)

{

  /* Infinite loop */

  while (1)

  {

// ilk olarak kullanacagimiz pinlerin bagli oldugu portun clock'unu belirlemeliyiz.

RCC_AHBPeriphClockCmd(RCC_APB2Periph_GPIOD,ENABLE);

// daha sonra port d den hangi pinlerin kullanilacagini , bu pinlerin clock'unu ve mod'unu belirlemeliyiz.

GPIO_initstructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 ;

GPIO_initstructure.GPIO_Mode = GPIO_Mode_Out_OD;

GPIO_initstructure.GPIO_Speed = GPIO_Speed_50MHz;

// bu kadar ayarlama pin ayarlarini yapmak için yeterlidir. Simdi biz bu ayarlar1 kaydetmek zorundayiz. Daha sonra program calisacaktir.

GPIO_Init(GPIOD,&GPIO_initstructure);

// böylelikle pin ayarlamasi bitti . simdi bu pinlerle ne yapacagimizi bulmaliyiz.

while(1)

{

GPIO_SetBits(GPIOD,GPIO_Pin_13);

GPIO_SetBits(GPIOD,GPIO_Pin_14);

delay();

GPIO_ResetBits(GPIOD,GPIO_Pin_13);

GPIO_ResetBits(GPIOD,GPIO_Pin_14);

delay();

}

  }

}

 

#ifdef  USE_FULL_ASSERT

 

/**

  * @brief  Reports the name of the source file and the source line number

  *         where the assert_param error has occurred.

  * @param  file: pointer to the source file name

  * @param  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{ 

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

 

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

But when I load the code to the board , nothing happens. So I debugged the code but in debug , program not exist below code part. How can I solve this problem ? 

do

  {

    HSEStatus = RCC->CR & RCC_CR_HSERDY;

    StartUpCounter++;  

  } while((HSEStatus == 0) && (StartUpCounter != HSE_STARTUP_TIMEOUT));
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    October 7, 2013
    Posted on October 07, 2013 at 13:18

    RCC_AHBPeriphClockCmd(RCC_APB2Periph_GPIOD,ENABLE);

    Not AHB then.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    sukrubahadirarslan
    Associate II
    October 8, 2013
    Posted on October 08, 2013 at 19:49

    thank you clive but still this code doesnt work and problem is same . Have you any suggestion ? 

    Tesla DeLorean
    Guru
    October 8, 2013
    Posted on October 08, 2013 at 20:13

    Well if you're attempting to start the HSE, and it's not starting, then you need to examine the board, and the signal at the oscillator. Make sure there are no jumper or solder-bridge settings related to the clock source.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..