Question
Preload for output compare for timer 1 - STM32F746
Posted on August 15, 2017 at 11:09
Hello,
I have a question to the note in the datasheet (RM0385 Rev 6, Page 682). Bit 3 OC1PE - Note 2.
What means this note?
'The PWM mode can be used without validating the preload register only in one
pulse mode (OPM bit set in TIMx_CR1 register). Else the behavior is not guaranteed.'We can use the preload only in one pulse mode. Is this correct? How can I validate the preload register?
Best regards,
Michael