Question
HS USB Device Won't Return Report Descriptor
Posted on February 06, 2015 at 13:32
I've got a STM32F405 using a Microchip USB3300 PHY set up to run as a HS HID USB device. The device gets MOST of the way through enumeration. However, when the host queries for the report descriptor, the device fails to respond. I have set a breakpoint and can verify that the device recognizes the request, and the request is correct. but it simply never returns the report descriptor. I have disabled any other interrupts to ensure they aren't causing the problem.
This same code executes fine on the STM32F427. As in: I don't even bother changing the target micro, I just run the same project built for the '405 on the '427, and it works fine. #stm32-usb-device