Skip to main content
NEERAJ GUPTA
Associate III
July 20, 2017
Question

Problems found in STM32F746NG USER MANUAL

  • July 20, 2017
  • 1 reply
  • 619 views
Posted on July 20, 2017 at 12:55

Refering to page no 167 in en.DM00124865.pdf  which is available as STM32F746NG USER MANUAL. 

These are following typo errors are found as follows:

Bit 10 ADC3EN: ADC3 clock enable

This bit is set and cleared by software.

0: ADC3 clock disabled

1: ADC3 clock disabled

Bit 9 ADC2EN: ADC2 clock enable

This bit is set and cleared by software.

0: ADC2 clock disabled

1: ADC2 clock disabled

Bit 8 ADC1EN: ADC1 clock enable

This bit is set and cleared by software.

0: ADC1 clock disabled

1: ADC1 clock disabled

Please! correct this also as soon as possible.

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    July 20, 2017
    Posted on July 20, 2017 at 14:51

    Hi

    GUPTA.NEERAJ

    ,

    I confirm these typo errors.

    This is already noted internally to be correct in the coming release of RM0

    Thanks and Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks