Skip to main content
armindavatgaran
Associate III
March 16, 2014
Question

stm32f4discovery connection with sd/mmc card

  • March 16, 2014
  • 1 reply
  • 590 views
Posted on March 16, 2014 at 22:17

Hello

I want to connect a SDcard to stm32f4discovery .

A typical sdcard has CMD , CLK , DAT[0:3] , GND & VDD pins .

how should this pins be assigned to SDIO related pins( D0...D6 , cmd & ck ) in stm32f407vgt6?

Can sdcard's power be supplied from stm32f4discovery? how ?

Thanks . 
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    March 16, 2014
    Posted on March 16, 2014 at 23:35

    Suggest you review some schematics, say the STM3240G-EVAL, and STM32F4-DIS-BB

    Based on the code I ported to the STM32F4-Discovery

     

    ''The Micro SD Slot/Socket is expected to be wired as follows

     

     

    CARDDETECT = PB15 (Retargetable)

     

    CLK = PC12

     

    CMD = PD2

     

    D0 = PC8

     

    D1 = PC9

     

    D2 = PC10

     

    D3 = PC11

     

    VDD = 3V

     

    VSS = GND

     

     

    PC10 (SCLK) and PC12 (SDIN) potentially conflict with the CS43L22''

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..