Skip to main content
arganasss
Associate III
May 9, 2014
Question

STM32f303 Output Compare

Posted on May 09, 2014 at 15:48

Hello, i'd like to do output compare on four pins: PE13, PE9 (LEDS), PA10 and PA12. Everyone works except PA12. I tried to do that with TIM16 and TIM4 with no luck. And i reconfigured the channels, i understand how they are mapped to pins (datasheet). So maybe someone knows why this happens? Here is the code. Thanks for your help.

#include ''stm32f30x.h''

TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStructure;

TIM_OCInitTypeDef TIM_OCInitStructure;

GPIO_InitTypeDef GPIO_InitStructure;

void Leds_config(void);

void Timer_config(void);

int main(void)

{

  // Enable clocks for E  and A ports

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE);

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);

  

  Leds_config();

  Timer_config();

    

  while(1)

  {

  }

}

void Leds_config(void)

{

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_13; // use 9 and 10 pins port E

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; // use alternate-function mode

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // High speed mode

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // Push-pull mode

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // don't use pull up resistors

  GPIO_Init(GPIOE, &GPIO_InitStructure); // write values to E port registers

  GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_2); // Connect timer1 to these IO pins

  GPIO_PinAFConfig(GPIOE, GPIO_PinSource13, GPIO_AF_2); 

  

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; // use 9 and 10 pins port E

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; // pin is in output mode

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // High speed mode

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // Push-pull mode

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // don't use pull up resistors

  GPIO_Init(GPIOA, &GPIO_InitStructure); // write values to E port

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_10); 

  

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; // 12 pin of PA.

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // High speed mode

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // Push-pull mode

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // don't use pull up resistors

  GPIO_Init(GPIOA, &GPIO_InitStructure); // write values to A port

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_10); 

}

void Timer_config(void)

{

  TIM_TimeBaseInitStructure.TIM_Period = 500-1; // Pulse period = 500us.

  TIM_TimeBaseInitStructure.TIM_Prescaler = 72-1; // Divide timer frequency 72Mhz/72Hz gives 1us ticks.

  TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; // Count from zero to ARR value.

  TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; // Dont divide timer clock

  TIM_TimeBaseInit(TIM1, &TIM_TimeBaseInitStructure);

  

  TIM_TimeBaseInitStructure.TIM_Period = 500-1; // Pulse period = 500us.

  TIM_TimeBaseInitStructure.TIM_Prescaler = 72-1; // Divide timer frequency 72Mhz/72Hz gives 1us ticks.

  TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; // Count from zero to ARR value.

  TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; // Dont divide timer clock

  TIM_TimeBaseInit(TIM2, &TIM_TimeBaseInitStructure);

  

  TIM_TimeBaseInitStructure.TIM_Period = 500-1; // Pulse period = 500us.

  TIM_TimeBaseInitStructure.TIM_Prescaler = 72-1; // Divide timer frequency 72Mhz/72Hz gives 1us ticks.

  TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; // Count from zero to ARR value.

  TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; // Dont divide timer clock

  TIM_TimeBaseInit(TIM4, &TIM_TimeBaseInitStructure);

  

    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 350;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  

  TIM_OC1Init(TIM1, &TIM_OCInitStructure);

  TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable );

  

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 20;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  

  TIM_OC3Init(TIM1, &TIM_OCInitStructure);

  TIM_OC3PreloadConfig(TIM1, TIM_OCPreload_Enable );

  

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 350;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC4Init(TIM2, &TIM_OCInitStructure);

  TIM_OC4PreloadConfig(TIM2, TIM_OCPreload_Enable );

  

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = 150;

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

  TIM_OC2Init(TIM4, &TIM_OCInitStructure);

  TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable );

  

  TIM_CtrlPWMOutputs(TIM1, ENABLE);

  TIM_CtrlPWMOutputs(TIM2, ENABLE);

  TIM_CtrlPWMOutputs(TIM4, ENABLE);

  TIM_Cmd(TIM1, ENABLE );

  TIM_Cmd(TIM2, ENABLE );

  TIM_Cmd(TIM4, ENABLE);

}

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    May 9, 2014
    Posted on May 09, 2014 at 16:00

    For the STM32F3-DISCO board observe that solder bridges SB21,22 need to be MADE for the signals PA11 & PA12 to reach the P2 header.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    arganasss
    arganasssAuthor
    Associate III
    May 9, 2014
    Posted on May 09, 2014 at 16:03

    Also tried to do this on some random pins on B port and it also was successfull, so maybe PA12 or PA11 interacts with something which is not allowed or acceptable?

    arganasss
    arganasssAuthor
    Associate III
    May 9, 2014
    Posted on May 09, 2014 at 16:06

    Heh. My lack of experience of not knowing where to look. I was concentrating on the program so much that i didn't even think about hardware. Thanks Clive, now it works.