Question
STM32F4 Temperature Function With I/O on PC6
Posted on May 17, 2017 at 07:27
Hello:
Question 1:
A question that I cannot find an answer for. If I'm using PC6 (STM32F4) as a GPIO already, can I still configure and use the internal temperature sensor on ADC16?
Question 2:
Using the calibration constants stored in the device, and adding some extra calibration points if required, how accurate is the temperature sensor at ranges of -40C to +70C ?
Thanks...
Note: this post was migrated and contained many threaded conversations, some content may be missing.