Skip to main content
turboscrew
Senior III
September 10, 2017
Question

RM0351 RTC wakeup

  • September 10, 2017
  • 1 reply
  • 558 views
Posted on September 10, 2017 at 16:20

In the STM32L4x5/4x6 reference manual (and some other manuals too, like RM0090) the figure 374 shows that the RTC wakeup timer can be clocked with ck_apre, but the description of RTC_CR says that the alternate input is ck_spre.

Can someone confirm that the register description is right and the picture is wrong?

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    September 11, 2017
    Posted on September 11, 2017 at 17:02

    Hello

    Aaltonen.Juha

    ,

    I confirm the typo in the RTC block diagram picture.

    RTC_WUTR must receive 2 inputs :

    • One from WUCKSEL prescaler output
    • One from ck_spre (RTC_PRER synchronous prescaler output) and not from ck_apre which is a mistake in the block diagram.

    This is a known error reported internallyand will be fixed in coming releases of the reference manual (as for other series of manuals too).

    Thanks

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks