Skip to main content
definitely
Associate II
May 6, 2014
Solved

USART Configuration

  • May 6, 2014
  • 6 replies
  • 2665 views
Posted on May 06, 2014 at 02:22

Hello everyone I need to use USART2 from my STM32F3 but I can't make it work. Here is my code. If someone can find my error please help me. 

&sharpinclude ''stm32f30x.h''

 

/**************************************************************************************/

 

void RCC_Configuration(void)

{

  /* Enable GPIO clock */

  RCC->AHBENR |= RCC_AHBENR_GPIODEN;

 

  /* Enable USART clock */

  RCC->APB1ENR |= RCC_APB1ENR_USART2EN;

}

 

/**************************************************************************************/

 

void GPIO_Configuration(void)

{

 

  /* Connect PD5 to USART1_Tx */

  GPIOD->MODER |= 2 << ( 5*2 ); // [ 9:8 ] MODER4[ 1:0 ] = 10b Alternate function on 

// PIN C4

//GPIOC->OTYPER |= 1 << ( 5*1 ); // [ 4 ] OT4 = 1 Output as open drain

GPIOD->OSPEEDR |= 3 << ( 5*2 ); // [ 9:8 ] OSPEEDR4[ 1:0 ] = 11b 50 MHz High-speed on PIN C4

//GPIOC->PUPDR &= ~( 3 << ( 5*2 ) ); // [ 9:8 ] PUPDR4[ 1:0 ] = 0 No pull-up/down om PIN C4

GPIOD->AFR[ 0 ] |= 7 << ( 5*4 );

 

  /* Connect PD6 to USART1_Rx */

GPIOD->MODER |= 2 << (6*2);  // GPIO_Mode_AF

GPIOD->AFR[0] |= 7 << (6*4);  //  AF7

 

}

 

/**************************************************************************************/

 

void USART2_Configuration(void)

{

 

  /* USART resources configuration (Clock, GPIO pins and USART registers) ----*/

  /* USART configured as follow:

        - BaudRate = 9600 baud

        - Word Length = 8 Bits

        - One Stop Bit

        - No parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

  USART2->BRR = 72000000/9600;

USART2->CR1 &= ~USART_CR1_OVER8; // Oversampling mode = 16 

USART2->CR1 &= ~USART_CR1_M;  // Word length = 8 bits

USART2->CR1 &= ~USART_CR1_PCE;  // No parity

USART2->CR1 |= USART_CR1_TE;  // Transmitter enable

USART2->CR1 |= USART_CR1_RE;  // Receiver enable

USART2->CR1 |= USART_CR1_UE;  // USART enable

USART2->CR2 &= ~(USART_CR2_STOP_1 | USART_CR2_STOP_0);

}

 

/**************************************************************************************/

 

void OutString(char *s)

{

  while(*s)

  {

    while(!(USART2->ISR & USART_ISR_TXE)); // Wait for Empty

 

    USART2->TDR =(USART2, *s++);

  }

}

 

/**************************************************************************************/

 

int main(void)

{

  RCC_Configuration();

 

  GPIO_Configuration();

 

  USART2_Configuration();

 

  OutString(''This is an echo back test for USART1\r\n'');

 

  while(1) // Don't want to exit

  {

    uint16_t ch;

 

    while(!(USART2->ISR & USART_ISR_RXNE)); // Wait for Char

 

    ch  = USART2->RDR; // Collect Char

 

    while(!(USART2->ISR & USART_ISR_TXE)); // Wait for Empty

 

    USART2->TDR=(USART2, ch); // Echo Char

  }

}

 

/**************************************************************************************/

 

&sharpifdef  USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *         where the assert_param error has occurred.

  * @param  file: pointer to the source file name

  * @param  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

 

  /* Infinite loop */

  while (1)

  {

  }

}

&sharpendif

#usart-stm32f3
This topic has been closed for replies.
Best answer by Tesla DeLorean
Posted on May 06, 2014 at 04:14

Yes it is valid.

Ok, but what does that construct actually do? But If I try to change it to USART2 and PD5/PD6 does not work. If you can help me would be nice. Could it be that APB1 doesn't run at 72 MHz?

// STM32 USART2 LOOP (Tx PD.5, Rx PD.6) STM32F3xx - sourcer32@gmail.com
#include ''stm32f30x.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* Enable GPIO clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD, ENABLE);
/* Enable USART clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Connect PD5 to USART2_Tx */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_7);
/* Connect PD6 to USART2_Rx */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_7);
/* Configure USART Tx/Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
/**************************************************************************************/
void USART2_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USART resources configuration (Clock, GPIO pins and USART registers) ----*/
/* USART configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* USART configuration */
USART_Init(USART2, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART2, ENABLE);
}
/**************************************************************************************/
void OutString(char *s)
{
while(*s)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, *s++);
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART2_Configuration();
OutString(''This is an echo back test for USART2

'');
while(1) // Don't want to exit
{
uint16_t ch;
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); // Wait for Char
ch = USART_ReceiveData(USART2); // Collect Char
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, ch); // Echo Char
}
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d

'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif

6 replies

Tesla DeLorean
Guru
May 6, 2014
Posted on May 06, 2014 at 02:34

This is valid C?

USART2->TDR=(USART2, ch); // Echo Char

USART2->TDR =(USART2, *s++);

Sorry, really not interested in wading through register level code.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
definitely
Associate II
May 6, 2014
Posted on May 06, 2014 at 02:41

Yes it is valid. The problem is that I have a code that works with PC4 and PC5 (USART1) but I need to change it to USART2 which uses PD5 and PD6. I use this code for PC4 and PC5 and this totally works. 

#include ''stm32f30x.h''

 

/**************************************************************************************/

 

void RCC_Configuration(void)

{

  /* Enable GPIO clock */

  RCC->AHBENR |= RCC_AHBENR_GPIOCEN;

 

  /* Enable USART clock */

  RCC->APB2ENR |= RCC_APB2ENR_USART1EN;

}

 

/**************************************************************************************/

 

void GPIO_Configuration(void)

{

 

  /* Connect PC4 to USART1_Tx */

  GPIOC->MODER |= 2 << ( 4*2 ); // [ 9:8 ] MODER4[ 1:0 ] = 10b Alternate function on 

// PIN C4

//GPIOC->OTYPER |= 1 << ( 4*1 ); // [ 4 ] OT4 = 1 Output as open drain

GPIOC->OSPEEDR |= 3 << ( 4*2 ); // [ 9:8 ] OSPEEDR4[ 1:0 ] = 11b 50 MHz High-speed on PIN C4

//GPIOC->PUPDR &= ~( 3 << ( 4*2 ) ); // [ 9:8 ] PUPDR4[ 1:0 ] = 0 No pull-up/down om PIN C4

GPIOC->AFR[ 0 ] |= 7 << ( 4*4 );

 

  /* Connect PC5 to USART1_Rx */

GPIOC->MODER |= 2 << (5*2);  // GPIO_Mode_AF

GPIOC->AFR[0] |= 7 << (5*4);  //  AF7

 

}

 

/**************************************************************************************/

 

void USART1_Configuration(void)

{

 

  /* USART resources configuration (Clock, GPIO pins and USART registers) ----*/

  /* USART configured as follow:

        - BaudRate = 9600 baud

        - Word Length = 8 Bits

        - One Stop Bit

        - No parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

  USART1->BRR = 72000000/9600;

USART1->CR1 &= ~USART_CR1_OVER8; // Oversampling mode = 16 

USART1->CR1 &= ~USART_CR1_M;  // Word length = 8 bits

USART1->CR1 &= ~USART_CR1_PCE;  // No parity

USART1->CR1 |= USART_CR1_TE;  // Transmitter enable

USART1->CR1 |= USART_CR1_RE;  // Receiver enable

USART1->CR1 |= USART_CR1_UE;  // USART enable

USART1->CR2 &= ~(USART_CR2_STOP_1 | USART_CR2_STOP_0);

}

 

/**************************************************************************************/

 

void OutString(char *s)

{

  while(*s)

  {

    while(!(USART1->ISR & USART_ISR_TXE)); // Wait for Empty

 

    USART1->TDR =(USART1, *s++);

  }

}

 

/**************************************************************************************/

 

int main(void)

{

  RCC_Configuration();

 

  GPIO_Configuration();

 

  USART1_Configuration();

 

  OutString(''This is an echo back test for USART1\r\n'');

 

  while(1) // Don't want to exit

  {

    uint16_t ch;

 

    while(!(USART1->ISR & USART_ISR_RXNE)); // Wait for Char

 

    ch  = USART1->RDR; // Collect Char

 

    while(!(USART1->ISR & USART_ISR_TXE)); // Wait for Empty

 

    USART1->TDR=(USART1, ch); // Echo Char

  }

}

 

/**************************************************************************************/

 

#ifdef  USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *         where the assert_param error has occurred.

  * @param  file: pointer to the source file name

  * @param  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

 

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

But If I try to change it to USART2 and PD5/PD6 does not work. If you can help me would be nice.

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 6, 2014
Posted on May 06, 2014 at 04:14

Yes it is valid.

Ok, but what does that construct actually do? But If I try to change it to USART2 and PD5/PD6 does not work. If you can help me would be nice. Could it be that APB1 doesn't run at 72 MHz?

// STM32 USART2 LOOP (Tx PD.5, Rx PD.6) STM32F3xx - sourcer32@gmail.com
#include ''stm32f30x.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* Enable GPIO clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD, ENABLE);
/* Enable USART clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Connect PD5 to USART2_Tx */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_7);
/* Connect PD6 to USART2_Rx */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_7);
/* Configure USART Tx/Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
/**************************************************************************************/
void USART2_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USART resources configuration (Clock, GPIO pins and USART registers) ----*/
/* USART configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* USART configuration */
USART_Init(USART2, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART2, ENABLE);
}
/**************************************************************************************/
void OutString(char *s)
{
while(*s)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, *s++);
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART2_Configuration();
OutString(''This is an echo back test for USART2

'');
while(1) // Don't want to exit
{
uint16_t ch;
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); // Wait for Char
ch = USART_ReceiveData(USART2); // Collect Char
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, ch); // Echo Char
}
}
/**************************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d

'', file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Chirag Shah
Visitor II
June 2, 2018
Posted on June 02, 2018 at 11:05

I tried the exact same code for PA2->TX, PA3->RX but it doesn't seem to work. The device is stm32f303CB also to view the data I am using a USB to TTL converter and connection of the same is as follows:-

Converter                      STM32

RX               

--------->         TX

TX               

--------->         RX

GND            

--------->         GND

3.3V             --------->         3.3V

The change done by me is as follows:-

GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7);

/* Connect PD6 to USART2_Rx */

GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7);

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;

/* Enable GPIO clock */

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

I am new to arm based devices do let me know where I might be going wrong.

Tesla DeLorean
Guru
June 3, 2018
Posted on June 03, 2018 at 17:52

The message was stuck in moderation, an off-board conversation indicates this has been resolved.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
definitely
Associate II
May 6, 2014
Posted on May 06, 2014 at 04:22

You are right Clive it was the frequency I changed it to the 36MHz that is needed to work and I did it. Thanks Very Much Man