Skip to main content
alexandre239955_stm1
Associate
February 11, 2016
Question

STEVAL-MKI109V1 recovery image

Posted on February 11, 2016 at 17:24

Hi, I've tried to upgrade the firmware via DfuSe Demo, but it hung

After this, I've discovered that my STEVAL-MKI109V1 board has bricked.

I can flash it again using a Nucleo Board's embedded STLink. I could test it and I've read the memory contents, so I am very confident about being able to write a binary on it.

Is there someone who could send me a binary image for this board?

PS: I've tried to extract .hex images from .dfu files inside ''stsw-mki109w.zip'', but all of them are bigger than 64kB (the size of STM32F102R8T6 that is on MKI109V1 board)
This topic has been closed for replies.

1 reply

louda.marian
ST Employee
July 14, 2016
Posted on July 14, 2016 at 16:22

Hello,

don't worry about size of hex file, it's size is many times higher than size of binary data. Try to program STEVAL-MKI109V1 with hex file you obtained from dfu file for example using ST-Link Utility.

Best Regards,

Marian