Skip to main content
yavar_zarei
Associate III
October 18, 2014
Question

Can I replace CMSIS ver4.20 on older versions of CMSIS files in standard peripheral library for stm32F10x and stm32F4x?

  • October 18, 2014
  • 1 reply
  • 573 views
Posted on October 18, 2014 at 08:06

Can I replace CMSIS ver4.20 files on older versions of CMSIS files in standard peripheral library for stm32F10x(ver3.5 or 3.6) and stm32F4x(ver1.4)?

Is there any bug in this change?

Is there any relation between SPL driver  files and CMSIS?
    This topic has been closed for replies.

    1 reply

    Montassar BEN ROMDHANE_O
    Visitor II
    October 20, 2014
    Posted on October 20, 2014 at 14:04

    Hi Mohsen,

    You can use the new CMSIS Version 4.2, instead of other versions, but you've to keep the Device folder (related to ST) as it is. You have to change only folders related to the Core, and normaly there is no direct dependency SPL/CMSIS versions. 

    Regards,

    Heisenberg.