Associate III
March 13, 2014
Question
One Pulse Mode with STM32F429DiscoveryBoard
- March 13, 2014
- 4 replies
- 1029 views
Posted on March 13, 2014 at 11:45
Hallo together,
I want to use Timer 1 to capture a logic high input at Pin A9 and to create an output signal at Pin A10.I have written the following code which is derived from an STM32F10x example.I do not get any output signal at PA10.Would be nice if someone could tell me what is wrong with my code!Thanks in advance.Code can be seen attached in Tim_13_3.txtAdditional questions:In the end I want to produce 2 pulses where the duration of the first one is dependent on a changing value and the second pulse is fixed. The delay between the first and second pulse is also fixed. Do you know any possibility except the delay function how this double pulse could be built up with high precision (+/- 0.5 microseconds)?Thank you,Best regards, Patrick #f4-!=-f1