Skip to main content
jhhong
Visitor II
December 15, 2017
Question

Low speed Control Problem of BLDC Motor by FOC SDK 4.3

  • December 15, 2017
  • 1 reply
  • 831 views
Posted on December 15, 2017 at 03:03

Hi

Now I tried to activate Low Voltage BLDC Motor(Model : Shinano LA052-080E3NL1) using by 'STM32F PMSM single/dual FOC SDK v4.3'.

The hardware configuration is following below :

     Control Board : STM32303C-EVAL

     Power Stage : STEVAL-IHM023V2

     BLDC Motor : LA052-080E3NL1

As follow instruction in user manual, I could activated BLDC Motor.

in this point, I have some questions about FOC SDK 4.3.

question 1)

     But, BLDC Motor couldn't run in low speed using by sensorless FOC Control and sixstep control method.

     Is it avoidable problem of BLDC Motor or did I something miss?

question 2)

     What is the ''Stop Ramp'' function in monitor of ST Motor Workbench?

     I didn't see this function working when I click that button. even it dosen't exactly descrived in user manual.

     0690X00000609EuQAI.png

question 3)

     is there exist 'sensored FOC control of BLDC' in 'STM32F PMSM single/dual FOC SDK v4.3'?

Thanks.

#foc-sdk-4.3.0 #bldc
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 22, 2021

The question has been moved to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards