Skip to main content
ffr3akk
Associate II
September 2, 2017
Question

STM32F7 SDRAM: corrupt data read

  • September 2, 2017
  • 2 replies
  • 972 views
Posted on September 02, 2017 at 02:02

I'm implementing a delay line and saving its buffer to SDRAM (starting from address0xC0000000)

#define AUDIO_REC_START_ADDR (SDRAM_WRITE_READ_ADDR + SRAM_WRITE_READ_ADDR_OFFSET)
#define AUDIO_BUFFER_IN AUDIO_REC_START_ADDR
#define AUDIO_BUFFER_OUT (AUDIO_BUFFER_IN + (AUDIO_BLOCK_LENGTH * 2 * sizeof(q15_t)))
#define DELAY_BUFFER_START (AUDIO_BUFFER_OUT + (AUDIO_BLOCK_LENGTH * 2 * sizeof(q15_t)))
#define DELAY_MAX_SECONDS 1
#define DELAY_BUFFER_LENGTH (DEFAULT_AUDIO_IN_FREQ * 2 * DELAY_MAX_SECONDS) // stereo�?�?�?�?�?�?

If I write to the delay buffer in SDRAM and immediately read from it, the data is fine, but if I need to read from the buffer in following cicles of the main loop (as needed for the delay line) the data turns out to be corrupted.

What is the best way of storing data in SDRAM so that those locations are not overwritten?

#sdram #stm32f746
This topic has been closed for replies.

2 replies

AVI-crak
Senior
September 2, 2017
Posted on September 02, 2017 at 02:23

Why is it so difficult to program a simple data file?

#define SDRAM           __attribute__((section('.qsdram')))

SDRAM  uint16_t audio_data[audio_zize];

ffr3akk
ffr3akkAuthor
Associate II
November 13, 2017
Posted on November 13, 2017 at 01:42

Late reply... anyway the strange behaviour I get is that when Ireference the arrays in sdramvianamed section

__attribute__((section('.sdram')))

the data is distorted, despite the arrays having the same addresses as when they were mapped manually.

Maybe I didn't add the sdram section correctly in the LinkerScript (attached)

________________

Attachments :

STM32F746NGHx_FLASH.ld.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy15&d=%2Fa%2F0X0000000b5m%2FEwRAG_k.FIpIk0lfPigiR4IK9BvOcTb2N0qV57bW2i8&asPdf=false