Skip to main content
amine
Associate II
March 17, 2014
Question

U-boot on STM32F4-DISCO

  • March 17, 2014
  • 4 replies
  • 1322 views
Posted on March 17, 2014 at 20:36

Hello everyone,

I am trying to make U-boot work on my STM32F4-discovery board, and I downloaded the Emcraft version which supports the STM32F429-Disco board. I have made the required modifications (I hope) but I am facing a weird problem where I receive corrupt chars from the serial port. I even tried the pre-built image provided and I have the same problem.

any one have an idea about what might be the problem, I am really confused here and ran out of possible explanation.

any help would be appreciated.
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    March 17, 2014
    Posted on March 17, 2014 at 20:54

    Using which USART/pins, because PA9 is not viable on the STM32F4-DISCO without modification.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    amine
    amineAuthor
    Associate II
    March 17, 2014
    Posted on March 17, 2014 at 21:18

    using that pin (PA9) it is made as the default pin in that setup by Emcraft.

    what pin can I use without problems, and what r the modifications I need to make?

    thanks

    Tesla DeLorean
    Guru
    March 17, 2014
    Posted on March 17, 2014 at 23:00

    You might be able to use USART6 via PC6/7

    For PA9 you should review the circuit diagram to see what is attached to it, the biggest problem is a large bulk capacitor, but it's connected to other USB related pins/chips too.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    amine
    amineAuthor
    Associate II
    March 18, 2014
    Posted on March 18, 2014 at 20:40

    that was the problem, and USART6 worked :)

    thanks a lot for your help.