Skip to main content
gaokushuai
Visitor II
February 26, 2014
Question

Flash Loader Demo unable to erase stm32f207vg

  • February 26, 2014
  • 2 replies
  • 732 views
Posted on February 26, 2014 at 11:08

When i use the flash demo to erase my mcu, i selected erase all and click Next, flash demo tell me ''FAIL: Unable to erase flash''.

What's wrong? Where can I get more information about it?

thanks.

0690X00000602rLQAQ.jpg   
    This topic has been closed for replies.

    2 replies

    troy1818
    Associate III
    February 26, 2014
    Posted on February 26, 2014 at 11:54

    Hi Gao Si,

    I think you need to be a little more specific. It is hard to help with only this little information. What board are you using? exactly what tools do you flash with? etc.

    Regards,

    /rygelxvi  
    Tesla DeLorean
    Guru
    February 26, 2014
    Posted on February 26, 2014 at 16:38

    I think you need to be a little more specific. It is hard to help with only this little information.

     

    I suspect that's the OP's POINT.

    I would look at what options and write protect settings have been applied to the part. Consider using the ST-LINK utilities? Or what you might have done to the part prior to this issue.

    Connect using 9600 8E1 (Even Parity)

    Try using the command line version, it might provide additional information.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..