Associate
November 13, 2015
Question
SD ADC behaviour on STM32F373
- November 13, 2015
- 2 replies
- 881 views
Posted on November 13, 2015 at 04:41
Hello,
I am using STM32F373RBTx micro in my prototype board and have an unexplained behaviour that I observed during my bench testing, particularly around SD ADC operation. 2 things were observed: 1. unexplained square-wave like signal on the ADC pin (scoped on PB2 pin) like shown in the attached plot. This is with the Sigma Delta ADC sampling rate set to 0.24ms. 2. unexplained current sink on PB2 pin which is significantly bigger than other ADC pins. For some reason, it is sinking ~1uA on constant DC voltage where other ADC pins with similar circuit configuration are sinking significantly lower current (~0.02uA - 0.4uA). I can't see anything mentioned about the current sinking capability on the datasheet and the only unique thing I can find about PB2 pin is that it is shared between SDADC1 and SDADC2 AIN. The current sinking issue does not appear on an unprogrammed micro. Both were observed with the SD ADC functioning. The square-wave signal like issue might be related to the way the sampling was set to but it is intriguing that it affect the input signal although it is set to be an input pin. Has anyone observed the same thing described above or any ideas on what causes the aforementioned behaviour?